TDK Electronics · TDK Europe

Piezo Solutions

Discover the broad portfolio of TDK piezo solutions

PZT, or lead zirconate titanate, is one of the world’s most widely used piezoelectric ceramic materials. It is a metallic oxide and its outstanding properties have been first discovered at the Tokyo Institute of Technology around 1952. Compared to the previously discovered piezoelectric material barium titanate, PZT allows higher operating temperatures and exhibits a much stronger piezoelectric effect. 

TDK is using three different basic technologies to manufacture piezoelectric devices:

 Intro Col 1 Pic

Single layer types

which are mainly used for sensors, actuators or buzzers and which traditionally are manufactured by pressing technology or tape casting

 Intro Col 2 Pic

Multi-layer types

incorporating internal electrodes made of AgPd or Cu are used for example for actuators or speakers

 Intro Col 3 Pic

MEMS based devices

for time-of-flight measurement

With manufacturing locations for piezo components in Europe as well as in Asia, TDK is focusing on high-volume production for the global market. We offer standard products as well as customized solutions and we continuously expand our product offering with new innovative modular solutions.


Our strength

Innovative modular solutions

 Innovative Pic BG

Piezoelectric components typically come in standardized shapes, like disks, stacks, tubes, or bimorph benders. Usually, these devices have not been designed with specific applications in mind. This makes the integration into new applications troublesome.

TDK is aiming beyond such generic components: We offer modular solutions based on piezoelectric elements, designed with a specific application in mind.

Some examples: amplified actuators, miniaturized ultrasonic sensors modules, PiezoListen™ and powder level sensors.

More on these products

Copper multilayer technology

 Copper Pic BG

Multilayer piezoelectric devices consist of multiple layers of piezoelectric material alternating with internal electrodes. While AgPd is the industry standard as material for the inner electrodes, TDK is the only company in the market that in addition is processing copper as alternative inner electrode material for mass production since decades.

Which advantages does the use of copper offer?

High-volume production & customized solutions

 High Volume Pic BG

Manufacturing piezoelectric devices generally involves three main steps:

  • First the powder needs to be prepared. 
  • After this, the product has to be brought into the required shape, making use of pressing or tape-casting technology. 
  • Finally sintering is creating a solid ceramic material with the requested properties. 

TDK has been manufacturing piezoelectric devices for decades and has proven to be a world-class supplier for demanding applications like automotive, consumer, or even medical applications. Our focus is on mass production of standard components; however, we also offer customized solutions for high-volume applications. 

Did You Know?

Applications & Products

Ultrasonic Sensors

To measure distances the sensor emits an ultrasonic impulse and receives the reflected signal back from the target object. Ultrasonic sensors are time of flight (TOF) sensors, as they measure the distance to the target by measuring the time difference between emission and reception.


Solutions for Haptics

To generate vibrotactile haptic feedback on surfaces, e.g., on displays or for wearable devices, actuators are required. Many of today’s solutions make use of electromagnetic actuators which often limit the haptic feedback to simple clicks or boring vibrations. To generate more versatile haptic feedback, so-called high-definition haptics, a new generation of actuators is required. 

Piezoelectric actuators are perfect for creating high-definition haptics. This is mainly because of their short response time and large signal bandwidth. Moreover, piezo actuators come in a compact package combined with low power consumption and strong force. 

TDK offers two different product lines, specifically designed for haptic feedback:


Actuators and Elements

Piezoelectric actuators can come in a variety of form factors, like stacks, bimorph benders or simple discs.


Solutions for Sound

A piezoelectric speaker is a loudspeaker that uses the piezoelectric effect for generating sound. It can be a simple buzzer, or, as in the case of our PiezoListen family a complete ultrathin speaker:

In case you are interested take a look to our comprehensive solutions page:


Get in touch with the experts

Not found what you are looking for? Want to know more?

Please briefly describe your idea/requirement and fill out the contact form. Our piezo experts will get in contact with you. 

First name is required Vorname wird benötigt 名字是必需的 お名前は必須項目です。
Last name is required Nachname wird benötigt 需要填写姓氏 姓は必須項目です
E-mail is required E-Mail wird benötigt 需要使用电子邮件 電子メールは必須項目です。
Company is required Unternehmen wird benötigt 公司需要 会社名は必須項目です。
Country is required Land wird benötigt 所需国家 国名は必須項目です。
Message is required Nachricht wird benötigt 所需信息 メッセージは必須項目です。
Accepting the data usage is required Datennutzung muss akzeptiert werden 必须接受数据使用 データ利用を承諾することが必要
More information Weitere Informationen 了解更多 詳細情報

Sales Network & Sites

Vertriebsnetz & Standorte

销售网点和工厂

販売網 & 工場

See our worldwide sales offices.

More

Zu unseren weltweiten Vertriebsbüros.

Mehr

查看我们的全球销售办事处。

更多内容

世界各地の販売拠点をご覧ください。

関連資料

Social Media

Soziale Medien

社交媒体

ソーシャルメディア

Follow us on

LinkedIn X (Twitter)

Folgen Sie uns auf

LinkedIn X (Twitter)

关注我们

WeChat LinkedIn X (Twitter)

フォローしてください

LinkedIn X (Twitter)

Tradeshows & Events

Messen & Events

展览会

各種イベント

Experience TDK live!

More

Erleben Sie TDK live!

Mehr

现场体验TDK

更多内容

TDKのライブを体験しよう

関連資料