TDK Electronics · TDK Europe
TDK Solutions for

Industrial Automation

 header_SM
 header_XL

Industrial Automation

TDK is the market leader in passive components for power electronics.

We offer the technologically and economically best possible solution for all power ranges and requirement profiles.

 


Solutions for Variable Frequency Drives

 Titelbild

An increasing number of electric motors are controlled by frequency converters that vary voltage and frequency at the electric motor as needed. A variety of reasons, such as energy efficiency, precise control of speed and torque, reduced noise emissions, and an extension of the equipment's service life through reduced mechanical stress, speak in favor of this trend.

Frequency converters require passive components with the highest reliability and resilience during very long periods of use.


NTC NTC NTC u u u PTC L1 PE L2 L3 L1 PE L2 L3 N Input Protection Input Filters (EMI & LCL Filter) Rectifier Booster, DC Link &Chopper Circuit Output Filters(LC-dV/dT & EMI Filter) Inverter PS, Driver & Controller Eingangsschutz Eingangsfilterung(EMV- & LCL-Filter) Gleich-richter Booster, DC-Link &Chopper-Schaltung Ausgangsfilterung(LC-dV/dT & EMV-Filter) Umrichter Stromversorgung, Treiberschaltung und Controller 1 2 3 4 5

For details, please choose the function unit in the circuit above.



Solutions for Uninterruptible Power Supplies

 Titelbild

UPS systems are used to compensate for fluctuations in the power supply or to take over the power supply from a battery for a defined period in the event of a power failure. This allows machines and computers to be shut down in a controlled manner, data to be backed up or time to be bridged in order to put emergency units into operation.

The reliability of the UPS system and thus of its components is a key requirement.


N L3 L2 L1 PE N L3 L2 L1 PE u u u + PS, Driver & Controller InputProtection Input Filters(EMI & LCL Filter) Output Filters(EMI & LC Filter) DC/ACInverter DCLink Battery Charge/Discharge Stromversorgung, Treiberschaltung und Controller Eingangs-schutz Eingangsfilterung(EMV- & LCL-Filter) Ausgangsfilterung(EMV- & LC-Filter) DC/AC-Umrichter DC-Link Batterie-Ladung/-Entladung 1 2 3 3 4 5

For details, please choose the function unit in the circuit above.

DC Link and Battery Charge/Discharge

For the DC link of the frequency converter in UPS systems TDK offers a wide selection of capacitors and inductors, suitable for all conceivable combinations of frequency, ripple current and temperature. The batteries are charged and discharged with sometimes very high currents. To prevent damage to the system due to overload, the batteries must be safely disconnected via high-current contactors.



Solutions for Switch Mode Power Supplies

 Titelbild

Many applications require a DC voltage that is usually considerably below the level of the AC mains voltage. Switch-mode power supplies convert the mains voltage to the required DC voltage level energy-efficiently and precisely in a compact and weight-optimized design.

TDK offers the right components for the different topologies such as LLC, flyback or buck-boost as well as for the different semiconductor technologies and the associated switching frequencies and edge steepnesses.


u NTC, PTC u N L PE N L PE InputProtection Input Filters Rectification/PFC Conversion Output Temperature Sensing Control Board Eingangs-schutz Eingangsfilterung Gleichrichtung/BLK Wandlerbeschaltung Ausgang Temperaturmessung Controller 1 2 3 3 3 4

For details, please choose the function unit in the circuit above.

Rectification / PFC / Conversion / Output

For rectification, PFC stage and converter circuitry, TDK offers a wide selection of capacitors and inductive components, suitable for all conceivable variants of the circuit topologies used.



Solutions for Industrial Robots

 Titelbild

Robots are increasingly shaping the image of the working world. They relieve humans of dangerous, heavy and monotonous tasks in production and service. In addition to the classic manufacturing robot, familiar from the automotive and electronics industries, they are increasingly being used in logistics, distribution centers and hospitals. Humanoid robots will soon support humans in their everyday lives.

Passive electronic components must be reliable and as compact as possible.


Sensors

Robots must operate with the highest precision and repeatability. This requires appropriate sensors that detect angles and distances with high resolution and long-term stability. TDK offers an extensive range of sensors in different technologies for this purpose.



Solutions for Condition-based Monitoring / I4.0

 Titelbild

Predicting and diagnosing a machine’s health before it becomes problematic will become the mainstream in factories, but not limited to. Also wind turbines, trains and power equipment requires insights that can only come from having accurate and reliable data.

TDK focus on condition-based monitoring leverages next-generation technologies that enable effective and efficient monitoring of equipments, delivering high performance sensors that can lead to improvements in uptime, productivity and quality.

TDK has developed sensors, which detect state of health of the equipment and transfer this important information to the monitoring systems.


Solutions for Power Quality Solutions

 Titelbild

Increasing demand for electrical energy, energy saving and CO2 reduction are the main challenges. The increasing use of power electronics causes disturbances in the grid which must either be filtered out or compensated for in order to keep the grid efficient and stable. Systems for reactive power compensation (PFC) and solutions for active or passive filtering of harmonics are required for this purpose. Reducing reactive power and improving power quality saves costs and ensures reliable operation for power generators and energy consumers in low and medium-voltage grids.



Further Information


Get in contact

Sales Network & Sites

If you are interested in our products, you will find here an overview of our worldwide sales offices, which you can contact quickly and easily

More

Product Inquiry

Are you interested in our solutions? Please do not hesitate to contact us! We will be glad to help you.

More

Tradeshows & Events

Experience TDK live!

More

Social Media

Follow us on

LinkedIn X (Twitter)