TDK Electronics · TDK Europe

MediPlas

Advanced, eco-friendly sterilization* technology

 Intro Pic

MediPlas provides on-demand, in-situ sterilization by generating reactive species that effectively neutralize harmful microbes, including bacteria, viruses, fungi, and spores, across diverse surfaces.

Its low-temperature operation makes it ideal for sterilizing heat-sensitive materials such as plastics, electronics, and medical devices, delivering a faster, safer alternative to conventional methods like autoclaving or ethylene oxide (EtO).

How MediPlas works

 function

MediPlas operates through two core components: the reactor and the driver. The reactor uses dielectric barrier discharge (DBD) technology to generate reactive oxygen and nitrogen species (RONS), which are key to its decontamination capabilities.

The exact composition and concentration of RONS in the gas mixture are influenced by several factors, including:

  • Type and humidity of the input gas
  • Temperature within the reaction chamber
  • Power settings applied by the driver.

Thanks to its flexible design, the MediPlas system can be tuned to produce a customized gas composition tailored to your specific application – in real time. This adaptability allows you to modify the reactive environment during the decontamination cycle without changing hardware or adding chemicals.

Explore the possibilities with our MediPlas Evaluation Kit.

Innovative applications

Closed-loop systems

 1 Closed-loop Pic

For systems capable of self-sterilization without disassembly, known as Cleaning in Place (CIP). The MediPlas reactor maintains a continuous circulation of reactive gases, steadily increasing their concentration. After the sterilization cycle is completed, the reactive agents are filtered out.

Ideal for medical environments, MediPlas ensures sterility without damaging sensitive instruments,  preserving both safety and equipment longevity.

Batch setups

 2 Batch Pic

In batch configurations, medical instruments are placed inside a sealed chamber. The MediPlas reactor fills this chamber with reactive gases, ensuring comprehensive exposure across all surfaces.

Unlike traditional autoclaves, MediPlas operates at low temperatures, making it suitable for delicate items such as endoscopes, wound dressings, and stents. It also enables faster cycles, requires no added chemicals, and consumes less energy.

Plasma-activated water (PAW)

 3 Water Pic

MediPlas can ionize the air or gas surrounding water to produce a potent blend of reactive species, such as ozone (O₃), hydrogen peroxide (H₂O₂), and nitrogen oxides (NOx) – collectively known as Plasma-activated water (PAW).

These reactive species induce oxidative stress on microbial cells, damaging their membranes and internal structures, ultimately leading to microbial inactivation. PAW is widely used in medical and dental sterilization, food safety, and agriculture.


Unique benefits

In-situ supply

 Customizable

MediPlas generates reactive species on demand, eliminating the need for complex supply chains or storage of hazardous chemicals. This makes it a highly flexible and scalable solution for various environments.

Environment-friendly

 Sustainable

Designed with both sustainability and sensitivity in mind, MediPlas offers a low-temperature alternative ideal for delicate instruments such as endoscopes, wound dressings, and stents.

Compared to EtO and autoclaves, MediPlas is cleaner, chemical-free, and energy efficient – making it safer for users and the environment.
 

Lightning speed cycles

 Fast

Unlike EtO, MediPlas requires no extended aeration times after the sterilization cycle. This significantly accelerates turnaround times, improving workflow efficiency and reducing downtime.


Comparison with common sterilization methods

 Comparison Pic

MediPlas enables in-situ RONS generation, such as hydrogen peroxide, for cost-effective solutions in a fraction of the time compared to conventional cycles. This means it is a genuine alternative to ethylene oxide (EtO). 

Welcome to the MediPlas Evaluation Kit!

 Eval kit Pic Page 1
 Eval kit Pic Page 8

The MediPlas Evaluation Kit is designed to provide developers and technical teams with a hands-on environment to explore, test, and integrate the MediPlas system into their applications. Whether you are evaluating its capabilities for plasma-based sterilization, water treatment, or other advanced applications, this kit offers all the essential tools and documentation to get started quickly and effectively.

With intuitive setup instructions, sample code, and real-time data access, the Evaluation Kit empowers you to:

  • Understand the core functionalities of the MediPlas system
  • Simulate real-world use cases in a controlled environment
  • Accelerate development and integration cycles
  • Evaluate performance, reliability, and compatibility with your systems

This kit is ideal for R&D teams, system integrators, and innovators looking to harness the power of plasma technology in their solutions.
 

Contact us Download user guide

Library

Data sheets



Get in touch with the experts

Are you interested in MediPlas? Please briefly describe your application. Our experts will contact you.

First name is required Vorname wird benötigt 名字是必需的 お名前は必須項目です。
Last name is required Nachname wird benötigt 需要填写姓氏 姓は必須項目です
E-mail is required E-Mail wird benötigt 需要使用电子邮件 電子メールは必須項目です。
Company is required Unternehmen wird benötigt 公司需要 会社名は必須項目です。
Country is required Land wird benötigt 所需国家 国名は必須項目です。
Message is required Nachricht wird benötigt 所需信息 メッセージは必須項目です。
Accepting the data usage is required Datennutzung muss akzeptiert werden 必须接受数据使用 データ利用を承諾することが必要
More information Weitere Informationen 了解更多 詳細情報

Sales Network & Sites

Vertriebsnetz & Standorte

销售网点和工厂

販売網 & 工場

See our worldwide sales offices.

More

Zu unseren weltweiten Vertriebsbüros.

Mehr

查看我们的全球销售办事处。

更多内容

世界各地の販売拠点をご覧ください。

関連資料

Social Media

Soziale Medien

社交媒体

ソーシャルメディア

Follow us on

LinkedIn X (Twitter)

Folgen Sie uns auf

LinkedIn X (Twitter)

关注我们

WeChat LinkedIn X (Twitter)

フォローしてください

LinkedIn X (Twitter)

Tradeshows & Events

Messen & Events

展览会

各種イベント

Experience TDK live!

More

Erleben Sie TDK live!

Mehr

现场体验TDK

更多内容

TDKのライブを体験しよう

関連資料

*Disclaimer on sterilization terminology

The term “sterilization” as used throughout this website refers to the intended microbial inactivation capabilities of the MediPlas system. Achieving true sterilization – defined as the complete elimination of all forms of microbial life, including bacterial spores – depends on specific boundary conditions such as exposure time, concentration of reactive species, environmental parameters, and validation protocols. Users must ensure that operational settings meet the required standards for sterilization in their respective applications and regulatory environments.