The MDT software allows application-related parameters to be calculated for all available EPCOS ferrite cores and / or materials. It provides access to their digitized material data including their graphical representations. The user manual of the software contains a detailed description of all functions. The tool can be used as online version, tested in browsers like Google Chrome, Mozilla Firefox, Internet Explorer and Opera, or as download, developed for Windows 7 and 10. The online version does not offer the same comprehensive set of functions as the desktop version.
The ferrite material list was updated according to the EPCOS Data Book 2017 “Ferrites and Accessories”. The new high frequency material PC200 was added.
Among the features of the current MDT version are:
To support design-ins you will find the data sheets for all materials by applications under www.tdk-electronics.tdk.com/ferrite_materials.