TDK Electronics · TDK Europe

June 10, 2021

Film capacitors: TDK offers compact DC-link solution for PCB mounting in cylindrical shape

 Bild_Teaser_en

TDK Corporation (TSE:6762) presents its new B32320I* series of compact cylindrical DC-link capacitors for mounting on PCBs. They are designed for voltages of 450 V DC to 1300 V DC and cover a capacitance range of 6.5 µF to 260 µF. The current handling capacity IRMS is up to 27.6 A (10 kHz, 60 °C) and minimal ESR is 2.4 mΩ. The new DC-link capacitors are designed for a maximum hotspot temperature of 105 °C. The plastic housing corresponds to UL 94 V-0.

Depending on the model, the dimensions are between 35 mm x 53 mm and 60 mm x 120 mm. Due to their relatively tall insertion height compared with cubic capacitors, the new DC-link capacitors have low footprint requirements on the PCB in relation to their capacity. All models in the new series feature five pins, which ensures high current capability as well as high stability on the PCB.

Typical areas of application include frequency converters for drives, converters for photovoltaic and air conditioning systems and critical UPS systems.

Main fields of application

  • Frequency converters for drives
  • Converters for photovoltaic and air conditioning systems as well as UPS systems

Main features and benefits

  • Rated voltage of 450 V DC to 1300 V DC
  • Capacitance range from 6.5 µF to 260 µF
  • Compact dimensions of 35 mm x 53 mm and 60 mm x 120 mm
  • Minimal space requirements on the PCB

Further information on the products can be found at www.tdk-electronics.tdk.com/en/ac_capacitors.

 

 

About TDK Corporation

TDK Corporation is a world leader in electronic solutions for the smart society based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution and deliberately “Attracting Tomorrow.” It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2021, TDK posted total sales of USD 13.3 billion and employed about 129,000 people worldwide.



Media Contact

Uli Pecher | Head of Public Relations TDK Electronics AG Phone +49 89 54020-2244 Get in contact
Ralf Higgelke | Product Communication TDK Electronics AG Phone +49 89 54020-1378 Get in contact
Debbie Martin TDK Electronics Inc. Fountain Hills, AZ/USA Phone +1 480 836-4104 Get in contact
Candido Dall'Agnoll TDK Electronics do Brasil Ltda. São Paulo/Brazil Phone +55 51 3484-7007 Get in contact
Himalaya Baghel TDK India Private Limited Mumbai/India Phone +91 12 04 50 58 42 Get in contact
Kathy Xu TDK (Shanghai) Electronics Ltd. Phone +86 21 22 19 15 98 Get in contact
Pierre Gazull Tronic's Microsystems SA Phone +33 04 76 97 94 54 Get in contact

Stay Connected

Press Newsletter

We would be happy to keep you informed via e-mail. Please note that this service is for journalists only.

Register

Social Media