TDK Electronics · TDK Europe
MediPlas Cold Plasma Generator

Safe and Efficient Sterilization

 Header Pic SM
 Header Pic XL

Cold Plasma Sterilization

3.5 million cases①, 90,000 deaths, and 7 billion euros in costs② every year – these are the statistics for hospital-acquired infections (HAIs) in Europe published by the European Center for Disease Prevention and Control (ECDC). Not to mention the personal suffering of those affected and the grief of those left behind. That said, the ECDC estimates that up to 50% of HAIs could be prevented.

One of the main causes of healthcare-associated infections is the formation of biofilms in tubes, hoses, and catheters, e.g. during cardiac and urinary catheterization, dialysis, and mechanical ventilation. These biofilms remain from previous treatments as they are very difficult to remove or neutralize without wearing out the tubing.

With MediPlas, TDK has developed a technology that can remove these biofilms without the use of toxic input chemicals and/or high temperatures and pressures, such as in an autoclave. In addition, this technology saves time in the sterilization process itself.

Find out more about this outstanding technology and the applications that can be realized with it.

Main challenges

 1 Temperature Pic

High temperatures and pressures

Medical devices can be sterilized in autoclaves that operate at high temperatures and pressures. However, this wears down plastic parts such as breathing and dialysis tubes. This causes additional costs.

 2 Environment Pic

Environment

As an alternative to autoclaves, substances like ethylene oxide (EtO) can be used. However, EtO is mutagenic and carcinogenic③. The procurement and safe storage of such hazardous chemicals means additional decontamination time and expense.

 Safety Pic

Safety

Handling hazardous chemicals such as ethylene oxide exposes medical personnel to a high risk. In addition, the storage effort is high, which results in additional costs.

 3 Biofilm Pic

Biofilms

Biofilms in tubes, hoses, and catheters are a major cause of millions of hospital-acquired infections each year. They cannot be safely removed or inactivated using most of the techniques mentioned above.

The Solution: MediPlas

 Intro Pic

At room temperature and atmospheric pressure, MediPlas generates highly sterilizing gaseous media from non-toxic, abundant gases like air, oxygen, and moisture. The supplied gases are ionized by a non-thermal cold atmospheric plasma, causing them to recombine into new molecules and produce a highly reactive gas such as nitric oxide (NOₓ) and hydrogen peroxide (H₂O₂) which flows out of the outlet. 
 

Learn more


Why MediPlas?

 Customizable

Adjustable 

Excellent control over the required gas composition for your specific sterilization process.

 Temperature

Gentle

Low temperatures for moisture and heat-sensitive medical equipment, e.g. endoscopes, respirators.

 Sustainable

Sustainable

No more harmful substances and low power consumption.

 Fast

Faster

No more disassembling of the device.

 Low Cost

Cost-effective

Save time and operating costs by reducing cycle times to a fraction.

Discover MediPlas in detail in our design guide!

 Whitepaper Pic Page 1
 Whitepaper Pic Page 11

Read our design guide and application note to learn how TDK's MediPlas solution can help you tackle your sterilization challenges.

The design guide examines MediPlas and illustrates why this TDK solution is superior, combining effective sterilization with the efficient use of non-toxic, readily available input gases and the tunability of different output gases.

Get in contact

Are you interested in MediPlas? Please briefly describe your application. Our experts will be glad to help you.
 

First name is required Vorname wird benötigt 名字是必需的 お名前は必須項目です。
Last name is required Nachname wird benötigt 需要填写姓氏 姓は必須項目です
E-mail is required E-Mail wird benötigt 需要使用电子邮件 電子メールは必須項目です。
Company is required Unternehmen wird benötigt 公司需要 会社名は必須項目です。
Country is required Land wird benötigt 所需国家 国名は必須項目です。
Message is required Nachricht wird benötigt 所需信息 メッセージは必須項目です。
Accepting the data usage is required Datennutzung muss akzeptiert werden 必须接受数据使用 データ利用を承諾することが必要
More information Weitere Informationen 了解更多 詳細情報

Sales Network & Sites

Vertriebsnetz & Standorte

销售网点和工厂

販売網 & 工場

See our worldwide sales offices.

More

Zu unseren weltweiten Vertriebsbüros.

Mehr

查看我们的全球销售办事处。

更多内容

世界各地の販売拠点をご覧ください。

関連資料

Social Media

Soziale Medien

社交媒体

ソーシャルメディア

Follow us on

LinkedIn X (Twitter)

Folgen Sie uns auf

LinkedIn X (Twitter)

关注我们

WeChat LinkedIn X (Twitter)

フォローしてください

LinkedIn X (Twitter)

Tradeshows & Events

Messen & Events

展览会

各種イベント

Experience TDK live!

More

Erleben Sie TDK live!

Mehr

现场体验TDK

更多内容

TDKのライブを体験しよう

関連資料