TDK Electronics · TDK Europe

LeaXield – Active Leakage Current Filter

​

Aggregate earth leakage currents can often cause RCDs (residual current devices) to trip at their threshold. As a result, RCDs are either not usable or only with substantial additional outlay.

TDK presents the LeaXield active leakage current filter, a novel electronic solution which facilitates a dramatic reduction of earth leakage currents. This enables the effective use of residual current devices (RCDs) and increases plant availability.


Usage

 LeaXield_Principle

A complete drive system consists of an EMC input filter, the frequency converter and the motor. LeaXield is connected between the RCD and the EMC input filter, and feeds the leakage currents back to the source, preventing them from flowing through the RCD and tripping it unintentionally.

Thanks to its compact dimensions, LeaXield is also ideal for retrofitting into existing systems. Furthermore, as no external voltage supply is necessary for operation, the installation costs are low.


Function

 LeaXieldCurve
LeaXield is effective over a broad frequency range from 150 Hz to 30 kHz. The unfiltered leakage currents (red) are dramatically attenuated (green) when LeaXield is used. It effectively filters both stationary leakage currents ranging from 150 Hz to 1 kHz and variable leakage currents, which are typically between 1 kHz and 16 kHz. The latter are determined by the frequency of the converter. The earth leakage currents filtered by LeaXield (green) are significantly below the RCD tripping threshold (blue), thereby preventing unintentional tripping of the RCD.



Applications

Converter-based variable-speed drives, including

  • Pluggable devices
  • Pumps
  • Compressors
  • Conveyance systems

Can LeaXield solve my problem?

What is the maximum permissible current?

The rated current of the LeaXield is 50 A at a rated temperature of 50 °C. A short-term overload of 75 A for up to 3 minutes per hour, or 125 A for up to 30 seconds per hour, is permissible.

What type of power system and what voltages is LeaXield suitable for?

LeaXield is suitable for use in a 3-wire TN system. It cannot be used in a 2-line system. Types for 4-line systems are available on request. The rated voltage is 305/530V AC (50 Hz). In addition, a minimum voltage of 208/360V AC (50 Hz) is required for operation. Types with higher rated currents are available on request.

Which RCD should be used?

The unintentional tripping of a universal RCD (Type B/Type B+) can be prevented with LeaXield. There are two distinct types which differ in their tripping characteristics, i.e. with regard to the tripping threshold dependent on the frequency and the time delay.
It should be noted that, in accordance with EN 50178 / VDE 0160, variable speed drive systems are only permissible if type B/B+ RCDs are used.

What is the maximum leakage current within the time range?

The maximum leakage current that can be reduced with the aid of the LeaXield is 1 A (peak value). Care should be taken not to exceed this value. Higher leakage currents can result in malfunctions or destruction of the device. To ensure that the maximum leakage current of 1 A is not exceeded, a leakage current measurement over time is first necessary.

The block diagram shows a typical drive system consisting of EMC filter, inverter and motor. For the analysis, the aggregate current via L1, L2 and L3 shall be measured with a current probe on the line side of the EMC filter. All three phases are to be conducted through the current probe (marked in green in the block diagram). A residual current measuring device should be used for the evaluation. Alternatively, an oscilloscope can also be used.

Important: The residual current must always be measured across all phases and not to ground.

 Schema


The measurement example below shows the maximum leakage current that flows into the system/machine on the line side. The peak value is about 500 mA and is thus lower than the maximum permissible value of 1 A. In this case it is possible to use the LeaXield.

 Currents without


How high is the leakage current depending on the frequency?

The analysis of the leakage current over the frequency range provides information on whether the frequencies to be attenuated lie within the operating range of LeaXield, which extends from 150 Hz to about 30 kHz. No significant attenuation is possible in these ranges beyond the operating range of LeaXield. The current probe as described in question 4 is to be used for this measurement. For the analysis, a differential current measuring device can again be used, or also the FFT mode of an oscilloscope.

Please note that the attenuation characteristic of LeaXield is frequency-dependent. As a rule, leakage currents with a frequency of >1 kHz exhibit higher amplitudes than at lower frequencies. Accordingly, the attenuation of LeaXield was also designed to be greater in the range above 1 kHz. The measurement example below shows the frequency spectrum of the leakage current. The frequency components that are problematical for the RCD, in this case 150 Hz and 2 kHz, are within the operating range of the LeaXield (150 Hz – 30 kHz) where the use of LeaXield is possible.

 Compensation



PDF Number of lines Maximum leakage current (A) Rated current (A) Rated voltage (V AC)
3 1 50 305/530 (50 Hz)
new
4 1 50 305/530 (50 Hz)

In order to download up to 20 files together as zip, please mark them with the check box. To start the download, please click the Download button at the end of the list.

  • Application notes
  • Cautions and warnings
  • General information
  • Technical information
  • Operating manual
  • Quality and environment
  • Safety Instructions
  • Selector guide
  • EMC services and EMC laboratory
  • Symbols and terms
  • Important notes

In order to download up to 20 files together as zip, please mark them with the check box. To start the download, please click the Download button at the end of the list.


Explore more


Get in touch with the experts

Do you have any questions regarding LeaXield? Just send us your details and we will get back to you!
 

First name is required Vorname wird benötigt 名字是必需的 お名前は必須項目です。
Last name is required Nachname wird benötigt 需要填写姓氏 姓は必須項目です
E-mail is required E-Mail wird benötigt 需要使用电子邮件 電子メールは必須項目です。
Company is required Unternehmen wird benötigt 公司需要 会社名は必須項目です。
Country is required Land wird benötigt 所需国家 国名は必須項目です。
Message is required Nachricht wird benötigt 所需信息 メッセージは必須項目です。
Accepting the data usage is required Datennutzung muss akzeptiert werden 必须接受数据使用 データ利用を承諾することが必要
More information Weitere Informationen 了解更多 詳細情報

Sales Network & Sites

Vertriebsnetz & Standorte

销售网点和工厂

販売網 & 工場

See our worldwide sales offices.

More

Zu unseren weltweiten Vertriebsbüros.

Mehr

查看我们的全球销售办事处。

更多内容

世界各地の販売拠点をご覧ください。

関連資料

Social Media

Soziale Medien

社交媒体

ソーシャルメディア

Follow us on

LinkedIn X (Twitter)

Folgen Sie uns auf

LinkedIn X (Twitter)

关注我们

WeChat LinkedIn X (Twitter)

フォローしてください

LinkedIn X (Twitter)

Tradeshows & Events

Messen & Events

展览会

各種イベント

Experience TDK live!

More

Erleben Sie TDK live!

Mehr

现场体验TDK

更多内容

TDKのライブを体験しよう

関連資料