TDK Electronics · TDK Europe

Use of Cookies - Capacitor Life And Rating Application (CLARA)

This web-based tool uses so-called cookies in several places. These cookies serve to provide you with the best possible service. 

Cookie name    Validity/ Expiration dateDescription
AcceptConditionAs long as the Browser is open. Once the user closes the browser it will be deleted.Cookie that contains the information whether the important notes and license agreement has already been accepted in order to avoid repeated display
AspNetCore.Antiforgery.[GeneratedValue]As long as the Browser is open. Once the user closes the browser it will be deleted.Cookie that automatically creates an unique value in order to verifying the user to be able to do POST Forms inside the website, avoiding the ability of external users trying to exploid CLARA website forms inside outer webs
[PartNumber]_pdc As long as the Browser is not updated or deleted. Once it’s saved for the first time it will remain as long as the Software of the Browser is the same.Cookie (text value) that is used for identify the parameter link Product Center in order to redirect from CLARA website to TDK Electronics product page
table_1 to table_5 As long as the Browser is not updated or deleted. Once it’s saved for the first time it will remain as long as the Software of the Browser is the same.Cookie that is used to save HTML data to be printed later in the Life and Rating Application
[PartNumber]_comment As long as the Browser is not updated or deleted. Once it’s saved for the first time it will remain as long as the Software of the Browser is the same.Cookie (text value) associated to a part number in order to save comments from the user
[PartNumber]­_check As long as the Browser is not updated or deleted. Once it’s saved for the first time it will remain as long as the Software of the Browser is the same.Cookie (temporal boolean value) associated to a part number so the user can compare part numbers between them in Characteristics and Life time Simulator
CountryAs long as the Browser is not updated or deleted. Once it’s saved for the first time it will remain as long as the Software of the Browser is the same.Cookie only saved the first time the user access, CLARA saves in browser local storage a country from where the user is accessing CLARA website
RegionAs long as the Browser is not updated or deleted. Once it’s saved for the first time it will remain as long as the Software of the Browser is the same.Cookie only saved the first time the user access, CLARA saves in browser local storage a country region from where the user is accessing CLARA website
Print_htmlAs long as the Browser is not updated or deleted. Once it’s saved for the first time it will remain as long as the Software of the Browser is the same.Cookie (text value) that is used to generate HTML that is going to be used to print all the Characteristics from CLARA Website
partNumbersAs long as the Browser is not updated or deleted. Once it’s saved for the first time it will remain as long as the Software of the Browser is the same.Cookie (text array) saving the values selected to compare
simulator_result_jsonAs long as the Browser is not updated or deleted. Once it’s saved for the first time it will remain as long as the Software of the Browser is the same.Cookie that is used to save the values returned from the Macro API that simulates the results as a JSON, and then print them in a result table
UserIDAs long as the Browser is not updated or deleted. Once it’s saved for the first time it will remain as long as the Software of the Browser is the same.Cookie that is automatically generated once when the users access CLARA website for the first time. It’s a random Hash generated based on the current date and time. Used to save the User behaviour anonymously inside CLARA database.  It’s impossible to identify a backtrack from our servers to the User browser userID. All the user tracking data saved are anonymous per browser.  
SessionIDAs long as the Browser Tab of the website is open. Once the tab containing CLARA website is closed the storage is erased. Cookie that is automatically generated once when the users access CLARA website for the first time. It’s a random Hash generated based on the current date and time. Used to save the user behaviour anonymously inside CLARA database PER session.  It’s impossible to identify a backtrack from our servers to the user browser sessionID. All the user tracking data saved are anonymous per session.