Founded in 1954, TDK Electronics do Brasil is the only company in South America to develop and produce both aluminum electrolytic capacitors and film capacitors. These capacitors are found in all types of electrical or electronic circuits and have the most varied applications, such as automotive electronics, industrial, consumer and medical applications.
More information about TDK ElectronicsHuman Resources
+55 51 34 84 70 00
Rua Bernardo Joaquim Ferreira, 624
Parque dos Anjos
94190-000 Gravatai, RS
BRAZIL