TDK Electronics · TDK Europe
 Dame Bildschirm
 Messgeräte
 Antennen

EMC Laboratory

Reliable operation, maximum availability without downtime, satisfied users and no complaints - that is the goal of every device manufacturer and developer. One of the prerequisites for this is meeting the requirements for electromagnetic compatibility (EMC). It ensures the trouble-free operation of devices and systems working alongside and with each other in an electromagnetic environment that is becoming increasingly challenging as the density of applications increases.

TDK is your comprehensive partner in all areas of electromagnetic compatibility

  • EMC services in the field of electromagnetic emission and immunity
  • Not only tests, but solutions for your requirements
  • Main focus: Industry, automotive, power electronics
  • Competence at the current state of the art, cooperation in standardization
  • 60 years EMC service provider in Regensburg, accredited test laboratory since 1994
  • TDK product portfolio for ensuring electromagnetic compatibility

We have moved!

We have moved to Emmy-Noether-Str 8, 93055 Regensburg, and are now back in the lab available to provide you with our services.

Why not schedule an appointment with us and be one of our first clients?


Lab News

 Bild News 2 x

Verification of the new 10 m semi-anechoic chamber

As planned, the verification measurements for our large absorber chamber at the new location were carried out and completed at the beginning of October. For a test volume of 5 m in diameter and 3 m in height, the measurements conducted by Seibersdorf Laboratories yielded an excellent site attenuation value in accordance with CISPR 16-1-4 of ±3 dB across the 30 MHz to 1 GHz frequency range. We are also very satisfied with the verified performance for the 9 kHz to 30 MHz range (measured at a distance of 10 m or 5 m, depending on the test volume) as well as for frequencies above 1 GHz. Just over two weeks later, we were able to carry out our first customer project in the chamber successfully. 

 Bild News 3

The time has come: The TDK EMC Laboratory Regensburg is Moving

The last measurements for our customers in our 63-year-old anechoic chamber in the Wernerwerkstraße were done by end of July 2026. We are now using August and September to relocate the laboratory to Emmy-Noether-Straße 8, D-93055 Regensburg. The new, state-of-the-art 10-meter chamber will be virtually complete by end of August. Commissioning and final verification measurements will take place in September, allowing us to resume regular testing operations in October. Our automotive chamber for component testing will also be operational by then.

 Bild News 1

Extension of accredited scope and application fields

Since 2024 we can carry out immunity tests against fields in close proximity in accordance with IEC/EN 61000-4-39 on the basis of our laboratory accreditation. Some product standards were also included, such as the EMC product standards for solar inverters IEC/EN 62920 and conductive charging of electric vehicles IEC/EN 61851-21-1 and -21-2. For these applications, we are equipped with a bidirectional DC system with a power of up to 144 kW for EUT operation. We can also control charging stations with a vehicle simulator via the Control Pilot of the CCS plug.


DENPAFLUX

 Denpaflux 1 Pic

DENPAFLUX EMC services

DENPAFLUX provides EMC expertise that fits your development cycle. Get expert EMC validation within 3 business days to keep innovation moving, or rely on a single, reliable partner to manage EMC risk across your product development. With 400+ EMC reports successfully delivered to clients, we help hardware teams turn EMC from an unpredictable, costly risk into a planned and controllable milestone.

 Denpaflux Logo

Benefit of using DENPAFLUX Services:

  • Dedicated team of experts matched to your EMC challenges
  • Flexible pricing models with no hidden fees
  • EMC support across your entire hardware development
 Denpaflux 2 Pic

EMC expertise across your entire product lifecycle

Most EMC issues are not caused by a lack of effort, but by when and how EMC is addressed. 

DENPAFLUX brings structure and continuity to EMC work by embedding EMC engineering into the development process instead of treating it as a late-stage checkpoint. 

From early specifications to lab testing and in-field performance, EMC risks are identified, resolved, and documented across all phases.

EMC handled as an engineering discipline, not a last-minute fix.
 

Visit DENPAFLUX to learn more


Seminars and Conferences

 TAE Logo en

EMV-konforme Entwicklung von Schaltungen und Geräten

EMV-Störquellen – EMV-Entstörung – EMV-Design-Rules
Ostfildern, Germany, December 1 - 3, 2026
Lectures:

1. Eigenschaften linearer Bauelemente

2. Eigenschaften nichtlinearer Bauelemente

Date:Thursday, December 3, 2026, starting 8:30 am
Language:German
Speaker:Christian Paulwitz, Head of EMC Laboratory, TDK Electronics AG, Regensburg
Location: Online or Technische Akademie Esslingen, An der Akademie 5, 73760 Ostfildern
 TAE Logo en

Elektromagnetische Verträglichkeit (EMV)

Grundlagen, Messtechnik, CE Kennzeichnung
Ostfildern, Germany, February 16 - 18, 2027, starting 8:45 am
Language:German
Speaker:Christian Paulwitz, Head of EMC Laboratory, TDK Electronics AG, Regensburg
Location:Online or Technische Akademie Esslingen, An der Akademie 5, 73760 Ostfildern


 Breakout Absorber


EMC basics

Mounting instructions

  • Specify the interference sources (with emissions) and disturbed equipment (electrical equipment or components with limited susceptibility).
  • Assign the interference sources and disturbed equipment to zones (mounting positions), and separate these spatially from each other.
  • Plan the cabling in wiring categories according to emissions and susceptibility.

EMC has become an essential quality feature. Even in the development phase of the system, legally stipulated protection requirements and technical risks must be taken into consideration. The following information is important for producing the electromagnetic compatibility of the entire system1):
 

1. Filter casing with large-area connection to ground and other metal support construction

 Kapitel 1

For example, provide a common metallically bright mounting plate for filter and converter, fully ground and connect with large area of the switch cabinet at low inductance. If necessary, use short ground straps and EMC seals (for example, connection to switch cabinet doors).

2. Make a distinction between protective earth and ground

Make a distinction between:

  • the protective conductor connection of the EMC filter;
  • the large-area grounding of the filter, which is necessary for the interference suppression function of the filter.

3. Create connections in your system with the same reference potential

Create connections in your system with the same reference potential to reduce galvanically coupled interference. All metallic reference potential from casing, machine and system parts should be connected with low impedance, suitable for high frequency and as meshed as possible. Establish large-area metallic connections, use equipotential bonding bars and establish short connections over flat ribbon grounding cables.

Establish large-area metallic connections, use equipotential bonding bars and establish short connections over flat ribbon grounding cables.

There are:

  • Large-area conductive fixing:
  • Low-inductance connection (a rectangular copper flat ribbon cable is preferred over round conductors)
  • Short connections (rule of thumb: Length divided by width < 3)
 Kapitel 3

4. Keep noisy lines as short as possible!

Keep lines from source of interference as short as possible!

Examples:

  • Short connection from converter to EMC filter, ideally flanged filters to avoid emission.
  • Interconnections as short as possible between the converter output and motor (even to reduce asymmetric currents through parasitic capacitances of the cable shield).

5. Shielding of noisy lines

Disturbance-contaminated lines must be shielded!
Examples:

  • Interconnections between frequency converter and motor if a corresponding output filter is not used.
  • Connection between filter and converter on line side, as long as not directly flanged.
  • Please note that the shielding effect of differen

6. Large-area shield connection on both ends

Connect shielded lines on both sides and across large area with reference potential, as direct or close as possible to the casing inlet or outlet.

Use:

  • EMC-compliant cable glands (wrap-around contact)
  • EMC base plate
  • EMC shield rails with large area contacting of the cable shield by means of corresponding metal clamps.

Avoid shielded connections via stubs! (Twisted shielding braid; soldered cable lugs etc.)

 Kapitel 6_1
 Kapitel 6_2

Also ensure that there is an EMC-compliant cable gland on the terminal box of the motor. These must meet the degree of protection of the respective location of use. The motor terminal box must be made of metal. The connection between the cable gland and terminal box must cover a large area. When removing the coating, the corrosion protect must be re-applied, if necessary.

7. Place EMC filters close to the casing outlet

 Kapitel 7

Examples:

  • Mains connecting side of the filter protrudes out of casing opening. (Ensure shock hazard protection!)
  • Use of appropriate EMC filters
  • Use of corresponding case adjustments to achieve shield attenuation (upon request)

8. Separate noisy and "clean" lines

Provide spatial separation between lines contaminated with disturbances and "clean" lines (lines contaminated with disturbances includes lines between converter and filter, "clean" lines between mains connection and filter).

Avoid parallel running (reduction in coupled disturbances).

Ensure that signal and power cables are run with spatial separation between them in order to prevent coupling lines (recommended minimum distance 20 cm). If necessary, provide metal sheeting; ground this over a wide area.

Run crossings, where possible at a right angle and with spacing.

 Kapitel 8

9. Place lines close to grounded metal areas

To reduce interference couplings, run the lines as close as possible to metal sheeting, which is connected with the reference potential (mounting plates, switch cabinet casing, etc.)

Conductive lines should also be run as closely as possible to the reference potential (reduction in inductively coupled interference).

In order to improve electromagnetic compatibility, cable ducts, cable troughs and installation
pipes made of metal are to be preferred over plastic parts.

 Kapitel 9

10. Signal lines

For unshielded signal lines (supply and return conductors), use twisted 2-wire lines in order to keep the area between the conductors as small as possible (to avoid magnetic coupling). The same applies for avoiding cable loops.

11. Switched inductors

Switched inductors (such as contactors, relays, magnetic valves etc.) should be connected close
to the source of interference with corresponding suppressors.

12. Signal transmission

For control signals in the area of a high interference level, use corresponding switching technology, such as symmetrical transmission systems with twisted wire pairs in connection with data line chokes, transmit digital signals according to the RS-422 standard or in extreme cases, cross the interference area using optical fibres.

13. Pay attention to the installation location of the filters!

Assembly must as a general rule be performed in such a way that natural convection is not impaired. This includes taking louvres in the filter casing and sufficient spacing to other installations into consideration. Overhead assembly is generally excluded. In the case of special installation situations, testing of the thermal conditions is required in consultation with TDK.

14. Acoustic noise minimization

An essential frequency-dependent filter component is the choke with very different core materials. In AC applications, electroacoustic effects are to be expected. The materials and processing technologies used generate a reasonable noise level when maintaining the harmonic components according to the EN 50160 standard for use in industrial areas. These may increase considerably at higher harmonic components. In the case of sensitive applications, such as assembly in offices, consultation from TDK should be considered.

15. Motor lines and motor types

Output voltages are generated in converter applications, which have virtually right angled curve shapes. These are primarily characterised by the rate rise as a dv/dt value and the switching frequency of the converter. The cables and motors in the output network of the converter and their inductive and capacitive components basically define the EMC properties of the system. Resonances of cable and motor combinations can in many cases be found again as resonance of the interference voltage measurement at the converter input side.

The parasitic capacitances of the cable and motor should be given particular attention. While the parasitic capacitances of the motor are dependent on the design, cables are dependent on the insulation material, the cable structure and the type of shielding and particularly on the length. A higher frequency current flows through the earthed system parts depending on the switching frequency, the dv/dt value and the magnitude of the parasitic capacitances.

The following effects may occur here:

  • As the parasitic currents flow through the ground connections of the system, the total input currents in the filter is no longer equal to zero. This can lead from a certain magnitude of the parasitic current to saturation of the current-compensated chokes in the filter and consequently exceeds the permitted interference level. The interference voltage measurement should be performed at the installed systems.
  • The parasitic currents also flow via the filter casing and the capacitors connected in the filter to the source of interference. Impermissibly high currents can lead to overload of capacitors and therefore a hazard!
 Kapitel 15

1) The figures in the "Mounting instructions" were provided by Rittal GmbH Co. KG, Herborn as well as Invensys Systems GmbH EUROTHERM, Limburg/ Lahn

Downloads

Technical information

PDF - 3.9 MB Download

How to get there

Our Laboratory is located in the south-east of Regensburg, Emmy-Noether-Straße 8:

Google Maps


Contact EMC laboratory

You are interested in EMC services?

Please complete this form and send it to us including your concern (consultation, testing, e.g.), your industry and details/information regarding test object name, applicable standards, emission/immunity, specific operating conditions, supply connection (guide number, current, voltage), approximate height and weight, operating parameters of product, required additional laboratory equipment.

The responsible expert will contact you as soon as possible.
 

 Herr Paulwitz

Christian Paulwitz
Laboratory manager
Tel: +49 89 54020 3282

 Herr Scheck

Simon Scheck
Deputy laboratory manager
Tel: +49 89 54020 3277

First name is required Vorname wird benötigt
Last name is required Nachname wird benötigt
E-mail is required E-Mail wird benötigt
Company is required Unternehmen wird benötigt
Country is required Land wird benötigt
Message is required Nachricht wird benötigt