TDK Electronics · TDK Europe

Plant in Heidenheim

December 21, 2017

70 years of inductors and capacitors made in Germany

 Teaser_LG

Heidenheim is one of TDK's longest-standing facilities. Today, some 430 employees produce inductors and power capacitors at the 29,000 m² facility, of which approximately three quarters are shipped to customers in the automotive industry.

More than two thirds of the electronic components manufactured here are for the European market.

Over the years the focus of the plant has evolved from pure manufacturing to development, process design and logistics in order to support the company's global business. About 30 percent of the employees are now employed in these areas. Production processes and automation concepts developed in Heidenheim are used in all other plants for inductors and capacitors.

Growing percentage of sales with products for e-mobility

Among the components manufactured here are innovative PCC power capacitors for hybrid and electric vehicles. These components are built into the power supply units for electric motors, where they stabilize voltage, store energy and thus play a part in facilitating better vehicle acceleration. The share of products made in Heidenheim for cutting-edge e mobility applications currently stands at about 15 percent and is growing all the time.

 Figure_Products
Figure 1:

EPCOS high-power inductors and power capacitors and TDK ACT data line chokes are manufactured in Heidenheim.

Miniaturized data line chokes account for by far the largest number of units produced here. These inductors enable interference-free data exchange between in-vehicle electronic controllers. They are increasingly also being used in driver assistance systems and in both telematics and autonomous driving applications.

Investment in cutting-edge production concepts

Further process automation with cutting-edge machines and Industry 4.0 concepts are being employed for the production of power capacitors. For example, the plant is currently working on the installation of a fully automated production line with several robots.

 Figure_Production
Figure 2:

Production of power capacitors in Heidenheim.

Profile plant in Heidenheim

Products

Inductors
  • Signal use inductors
  • Power inductors
EMC filters
  • Data and signal line chokes
  • Design & Application Center for power EMC filters
Aluminum electrolytic and film power capacitors
  • Design & Application Center for aluminum electrolytic capacitors
  • Power capacitors
  • Components for power factor correction (PFC)

Certifications

  • ISO 9001
  • ISO/TS 16949
  • ISO 14001
  • ISO 50001

History

1947First production hall
1948Production of resistors and capacitors
1952Production of power capacitors
1956Production of leaded tantalum capacitors
1967More than 20 buildings on the site
1981Gas motor heat pump system – one of a kind in Germany – installed to boost operational energy efficiency
199610-millionth data line choke produced
2010One billionth data line choke produced
2011First production line for TDK ACT data line chokes
2016Work begins on construction of a fully automated production line for PCC LP power capacitors


Get in Contact

Sales Network & Sites

If you are interested in our products, you will find here an overview of our worldwide sales offices, which you can contact quickly and easily